You're reading the documentation for an obsolete version. For the latest released version, please have a look at v10.9.
4. ROS2 Namespace
To aid in differentiating between multiple robots, most ROS2 topics are prefixed with a namespace. The ROS2 message bus is capable of integrating multiple robots, sensors and other nodes on the same network, namespaces can prevent collisions in such scenarios.
Here are a few tips and tricks related to the namespace:
Namespace is constructed with a serial number prefixed with ‘UR’.
URCapX backend contributions running in docker containers can read namespace from ROS2_NAMESPACE environment variable
Topic names and namespaces should follow the ROS2 recommendation “snake case”.(https://design.ros2.org/articles/topic_and_service_names.html)
4.1 Example topic name with namespace
When serial number is “20225300015” the topic name would be:
/UR20225300015/speed_fraction
4.2 Exceptions
There are few topics that are not prefixed with namespace. Reason for that is to keep compatibility with ROS2 tools. These topics are:
joint_states
target_joint_states
tf
tf_static
All are published without namespace. In this case namespace string is prefixed to joint name. Example: name=”UR20225300015_elbow_joint”.